ApossC SDK  V01.15

Description of the idea and purpose of the SDK. The SDK allows a quick start with ApossIDE and simplifies the use of the tool. The SDK is written in ApossC. To guarantee the functionality of the provided functions, it is recommended to use the latest version of ApossIDE. As minimum requirement an ApossIDE version greater than 7.00.00 is required. In case of questions or ambiguities the support of Zub machine control ag can be contacted.

Contact
zub machine control AG
Buzibachstrasse 31
6023 Rothenburg
Switzerland
Phone +41 41 54150-40
E-Mail info-.nosp@m.zub@.nosp@m.maxon.nosp@m.grou.nosp@m.p.com

Data Sheets | Released Software | Software Manuals | Hardware Manuals | Maxon Shop

Maxon Support Center