ApossC SDK  V01.15
File List
Here is a list of all files with brief descriptions:
 SDK_Amplifier_DS402_StateMachine.mcThis file provides all the function used for DS402 PPM and PVM
 SDK_Amplifier_DS402_StateMachine.mhDeclaration of the DS402 StateMachineFunction
 SDK_Amplifier_Epos4.mcThis file provides all the function used to setup a Epos4 drive
 SDK_Amplifier_Epos4.mhDeclaration of the Epos4 function
 SDK_Amplifier_MACS.mcFunctions for the integrated amplifier setup
 SDK_Amplifier_MACS.mhDeclaration of the integreted amplifier functions
 SDK_Amplifier_MiniMACS6_DS402_Slave.mcThis file provides all the function used to setup a MiniMACS6 DS402 slave
 SDK_Amplifier_MiniMACS6_DS402_Slave.mhDeclaration of the MiniMACS6 DS402 slave function
 SDK_Amplifier_MotorAlignment.mcFunctions for aligning a motor
 SDK_Amplifier_MotorAlignment.mhDeclaration of the motor aligning function
 SDK_Amplifier_MotorCommissioning.mcFunctions for commissioning a motor
 SDK_Amplifier_MotorCommissioning.mhDeclaration of the motor commissioning functions
 SDK_ApossC.mcFile to include the entire SDK
 SDK_Axis_Setup.mcFunctions for the axis setup
 SDK_Axis_Setup.mhDeclaration of the axis setup function
 SDK_Bussystem_EtherCat.mcFunctions to work with an EtherCat Master/ slave
 SDK_Bussystem_EtherCat.mhDeclaration of the EtherCat functions
 SDK_Communication_Ethernet.mcFunctions to work with an Ethernet as communication
 SDK_Communication_Ethernet.mhDeclaration of the Ethernet functions
 SDK_Encoder_Setup.mcFunctions for the general amplifier setup
 SDK_Encoder_Setup.mhDeclaration of the encoder setup function
 SDK_Error_Description.mc
 SDK_Error_Description.mhDeclaration of Error Codes
 SDK_Information_General.mcFunctions to get general informations
 SDK_Information_General.mhDeclaration of the general information functions
 SDK_Kinematics_Setup.mcFunctions for the kinematics setup
 SDK_Kinematics_Setup.mhDeclaration of the kinematics setup function
 SDK_Miscellaneous_IO.mcFunctions with IO samples
 SDK_Miscellaneous_IO.mhDeclaration of the IO functions
 SDK_Miscellaneous_Recording.mcFunctions with recording samples
 SDK_Miscellaneous_Recording.mhDeclaration of the recording functions
 SDK_Motion_Movement.mcFunctions for the simplification of movements
 SDK_Motion_Movement.mhDeclaration of the motion movement functions
 SDK_SignalGenerator.mcFunctions for the operation of the signal generator
 SDK_SignalGenerator.mhDeclaration of the signal generator functions
 SDK_VirtualModule_AxisSetup.mcFunctions to work with virtual axis modules
 SDK_VirtualModule_AxisSetup.mhDeclaration of the virtual axis setup functions
 SDK_VirtualModule_MasterSetup.mcFunctions to work with a virtual master
 SDK_VirtualModule_MasterSetup.mhDeclaration of the virtual master functions
 SdoDictionary.mh
 ut_Control_Loop_Parameter_Slider.zbm
 ut_UserParamExchange_USB_V1-00.zbm

Data Sheets | Released Software | Software Manuals | Hardware Manuals | Maxon Shop

Maxon Support Center